CCS doesn't set breakpoint in mapped source file

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Composer Studio Theia
    • CCSNXT-3047
    • CCS_20.4.0
    • CCS_20.5.0
    • None
    • Workarounds include involve typing out the location of the breakpoint manually (either in the scripting console, or in a breakpoint creation dialog). In both cases, the breakpoint is set on the target but it does not appear in the source view.

      CCS doesn't set breakpoint in mapped source file.

      Workarounds include involve typing out the location of the breakpoint manually (either in the scripting console, or in a breakpoint creation dialog). In both cases, the breakpoint is set on the target but it does not appear in the source view.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6381 - CCS doesn't set breakpoint in mappe...
                SYNCHRONIZED
                • Last Sync Date: