Need PTPv1 support / fixes on AM62x family along with PTPv2

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Linux Core SDK
    • LCPD-44971
    • 11.01
    • 11.02
    • Hide
      am62pxx_sk-fs
      am62xx_sk-fs
      am62xx_sk-se
      am64xx-evm
      am64xx-hsevm
      Show
      am62pxx_sk-fs am62xx_sk-fs am62xx_sk-se am64xx-evm am64xx-hsevm

      PTPv1 support was added earlier, but later PTPv1 support was removed and only PTPv2 is supported currently. Audinate Dante DEP works only with PTPv1.  I have the fix for the same, we need to make sure that fixes can be made in upstream and maintained going forward.

      Would like this to be tracked for inclusion in SDK11.0 with potential CI/CD release sooner.

      PTPv1 can be tested using the Linux tool - tools/testing/self tests/net/timestamping

      Fix merged in upstream - https://lore.kernel.org/all/20250917041455.1815579-1-v-singh1@ti.com/

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6281 - Need PTPv1 support / fixes on AM62x...
                SYNCHRONIZED
                • Last Sync Date: