ptp4l gm_hsr0.cfg and oc_hsr0.cfg nonoffload example is deprecated

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Linux Core SDK
    • LCPD-45511
    • 11.01
    • 11.02
    • Hide
      am64xx-evm
      am64xx-hsevm
      Show
      am64xx-evm am64xx-hsevm

      The example given in "PTP Ordinary Clock" in https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/latest/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/Network/HSR_PRP_Non_Offload.html is deprecated, showing the following messages when running the example. 

      option slaveOnly is deprecated, please use clientOnly instead                    
      unknown option doubly_attached_clock at line 13 in global section                  
      failed to parse configuration file gm_hsr0.cfgunknown option redundancy at line 17 in hsr0 section                         
      failed to parse configuration file gm_hsr0.cfg unknown option redundancy_master_interface at line 23 in eth1 section
      failed to parse configuration file gm_hsr0.cfg 

      This suggests that ptp4l no longer uses these parameters and so the documentation has be updated with the appropriate parameters for running PTP over HSR or PRP nonoffload. 

      This issue was observed on CPSW Ethernet but should not be specific to CPSW and it could also occur on PRU-ICSSG Ethernet.

      Update 11/14/2025:

      This section in the SDK documentation should be removed if the PTP over HSR/PRP nonoffload example was a carry-over from older devices: https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/latest/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/Network/HSR_PRP_Non_Offload.html 

      Fix: https://github.com/TexasInstruments/processor-sdk-doc/pull/530

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6279 - ptp4l gm_hsr0.cfg and oc_hsr0.cfg n...
                SYNCHRONIZED
                • Last Sync Date: