Update installer should block installing on macOS catalina (10.15)

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-2972
    • CCS_20.4.0
    • CCS_20.5.0
    • None

      The Theia we include in CCSv20.4.0 detects if you are running on Catalina and blocks execution. This can be a problem for users who are updating an existing CCS installation. For example you can install CCSv20.3.0 on Catalina and it will run fine even though it is not supported. However if you then update to 20.4.0 your installation will be broken.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6327 - Update installer should block insta...
                SYNCHRONIZED
                • Last Sync Date: