Scanner cannot Find Device that Distributes IRK with Static Random Address after Bonding and Reset

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SimpleLink Lowpower SDK F3 BLE5 Stack
    • BLE_LOKI-3840
    • BLE_LOKI_9_14_00
    • Hide
      BLE_LOKI_9_14_02
      BLE_LOKI_9_14_02_RC1
      Show
      BLE_LOKI_9_14_02 BLE_LOKI_9_14_02_RC1
    • Hide
      CC23xx
      CC27xx
      Show
      CC23xx CC27xx

      Description: The advertiser uses a random static address and operates in connectable mode. The central device connects to the advertiser, and both devices exchange IRK keys. After the connection and IRK distribution, the advertiser continues advertising using the same random static address. The scanner ignores these advertising packets and does not send advertising events to the host.
      In this test case, the scanner ignores advertising packets from devices that have distributed their IRK and are resolvable but use their identity address even though their privacy mode is set to Network privacy mode.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6314 - Scanner cannot Find Device that Dis...
                SYNCHRONIZED
                • Last Sync Date: