AM62x: VTM Example and FT are failing in r5f-freertos

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Processors SDL
    • PROC_SDL-9478
    • PROC_SDL_SMPU_11.02.00
    • PROC_SDL_SMPU_11.02.00
    • am62xx-sk

      Sciserver Testapp Built On: Oct 23 2025 13:23:55
      Sciserver Version: v2025.10.0.0
      RM_PM_HAL Version: v11.02.00
      Starting Sciserver..... PASSED
      
       VTM Example Application
      
      VTM_ESM_init: Init MAIN ESM complete 
      
       VTM_ESM_init complete
      Starting Use Case 0 
      sensor id                       : 0 
      adc_code                        : 356 
      temp in milli degree celcius    : 47697 
      vtmTriggerTh: Setting lt_thr0_val temp to 43697 millidegrees Celsius, and adc_code_lt_thr0 = 338
      vtmTriggerTh: Setting gt_thr1_val temp to 45697 millidegrees Celsius, and adc_code_gt_thr1 = 348
      vtmTriggerTh: Setting gt_thr2_val temp to 52697 millidegrees Celsius, and adc_code_gt_thr2 = 378

      Above log is obtained in automation dashboard for example, and similar is obtained for FT. Program execution seems to be stuck. R5F freertos binaries are problematic.

      Considering the similarity between FT and example it is expected that the fix will be common

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6237 - AM62x: VTM Example and FT are faili...
                SYNCHRONIZED
                • Last Sync Date: