Support expression values when exporting/importing to/from JSON text file

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Unresolved
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-2944
    • Hide
      CCS_20.4.0
      CCS_20.3.1
      Show
      CCS_20.4.0 CCS_20.3.1
    • CCS_21.0.1
    • None

      The Watch view has the option to import/export expression names from/to a JSON text file. This request is to also support expression values. Allow the user the option to include the values on export. Also allow the user to choose if they wish to import the names and also write the associated values stored in the JSON file. If there are no values in the JSON file then only the names will be imported.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6136 - Support expression values when expo...
                SYNCHRONIZED
                • Last Sync Date: