"Device CC2340R5RHBQ1 not supported" error occurs when switching platform from CC2340R5 to CC2340R5-Q1

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Not Prioritized

      "Device CC2340R5RHBQ1 not supported" error occurs when switching the platform from  CC2340R5 to CC2340R5-Q1 with SysConfig version 1.24.1 and 1.25.0 using SDK 9.12. No issue with 1.23.2.

      This error is occurring because CC2340R5HB was updated to CC2340R5HBQ1 in newer versions of SysConfig. However, the mapping file in the Simplelink SDK was not updated.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6107 - "Device CC2340R5RHBQ1 not supported...
                SYNCHRONIZED
                • Last Sync Date: