DSI fails to reconnect after suspend/resume

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Linux Core SDK
    • LCPD-44700
    • 11.00
    • 11.01
    • am62lxx_evm-fs

      After suspend/resume of AM62L with a DSI system connected, Linux fails to connect back to the DSI system.

      The following is seen during resume of the system:

      [   30.477672] edt_ft5x06 0-0038: Unable to fetch data, error: -121 

      Fixed by: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/commit/?h=ti-linux-6.12.y-cicd&id=28fe7134779cecd2660ffc80c9fcbd863994ae34

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6049 - DSI fails to reconnect after suspen...
                SYNCHRONIZED
                • Last Sync Date: