AM6x - Sitara Socs MCASP and BCDMA issue.

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Linux Core SDK
    • LCPD-45149
    • Hide
      09.02.00
      10.00
      11.01
      11.00
      10.01
      Show
      09.02.00 10.00 11.01 11.00 10.01
    • 11.02
    • Hide
      am62axx_sk-fs
      am62axx_sk-se
      am62lxx_evm-fs
      am62lxx_evm-se
      am62pxx_sk-fs
      am62pxx_sk-se
      am62xx_lp_sk-fs
      am62xx_lp_sk-se
      am62xx_p0_sk-fs
      am62xx_sk-fs
      am62xx_sk-se
      am62xxsip_sk-fs
      am62xxsip_sk-se
      Show
      am62axx_sk-fs am62axx_sk-se am62lxx_evm-fs am62lxx_evm-se am62pxx_sk-fs am62pxx_sk-se am62xx_lp_sk-fs am62xx_lp_sk-se am62xx_p0_sk-fs am62xx_sk-fs am62xx_sk-se am62xxsip_sk-fs am62xxsip_sk-se

      Customer is reporting this issue with BCDMA. They reported that the code that sets bstcnt value is incorrect and have also attached a patch to resolve.

      The “bstcnt “ is based on a single TR, however the driver in udma_prep_dma_cyclic_tr() may generate one or two TR per cycle based on the size when calling udma_get_tr_counters()

      Ref patch and also address the below two queries:

       

      1. Is there a performance impact when the transfer is broken into two transfer requests and the second request is only 8 bytes?
      2. For the application of McASP to PDMA to BCDMA where is the packet length (period_len in k3-udma.c) of 64kB set?

      E2E:

      https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1559488/am623-udma-cyclic-mode-for-mcasp-broken-by-eop-change

      Patch code:

      Workaround for bug in commit 67d5b24398155d07376b04dd8b3d858d049a5e17
      Original commit title:
          dmaengine: ti: k3-udma: Fix teardown for cyclic RX with PDMAThe original commit sets EOP at the end of BCDMA transfer and sets bstcnt
      based on the contents of transmit resquest (TR) #0. The driver, however, will
      use two TRs when transfer size is >=64k bytes with EOP set on the second TR. 
      In this case bstcnt should equal the total bytes for both TRs.diff --git a/drivers/dma/ti/k3-udma.c b/drivers/dma/ti/k3-udma.c
      index 4291bbf998ab..81b62df45be2 100644
      --- a/drivers/dma/ti/k3-udma.c
      +++ b/drivers/dma/ti/k3-udma.c
      @@ -3220,6 +3220,11 @@ static int udma_configure_statictr(struct udma_chan *uc, struct udma_desc *d,
       
               d->static_tr.bstcnt =
                   (tr_req->icnt0 * tr_req->icnt1) / dev_width;
      +
      +        // Data may be in two TR if >=64k
      +        if( !(tr_req->flags & CPPI5_TR_CSF_EOP) ){
      +            d->static_tr.bstcnt += (tr_req[1].icnt0 * tr_req[1].icnt1) / dev_width;
      +        }
           } else {
               d->static_tr.bstcnt = 0;
           }

       
      Fix Details:
      https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/commit/?h=ti-linux-6.12.y&id=5b37c96ee1c865edd28f69f3c7ac637a93a3b068

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6040 - AM6x - Sitara Socs MCASP and BCDMA ...
                SYNCHRONIZED
                • Last Sync Date: