Project build can hang on build and doesn't properly display errors

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High

      Project build can hang on build and doesn't properly display errors for some compiler errors.

      There is no issue using the headless project CLI command to build the project.

      There is no issue at all with CCS 20.2.0.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            1 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5990 - Project build can hang on build and...
                SYNCHRONIZED
                • Last Sync Date: