Dwarf call frame information contains frame description entries with instructions with the wrong address

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Generation Tools
    • CODEGEN-14342
    • Hide
      C29_1.0.0.LTS
      C2000_22.6.0.LTS
      C6000_8.3.0
      MSP430_20.2.0.LTS
      C6000_8.5.0.LTS
      MSP430_21.6.0.LTS
      ARMCLANG_4.0.0.LTS
      ARMCLANG_3.2.0.LTS
      C2000_21.6.0.LTS
      PRU_2.3.0
      C7000_5.0.1.LTS
      ARMCLANG_5.0.0.LTS*
      Show
      C29_1.0.0.LTS C2000_22.6.0.LTS C6000_8.3.0 MSP430_20.2.0.LTS C6000_8.5.0.LTS MSP430_21.6.0.LTS ARMCLANG_4.0.0.LTS ARMCLANG_3.2.0.LTS C2000_21.6.0.LTS PRU_2.3.0 C7000_5.0.1.LTS ARMCLANG_5.0.0.LTS*
    • Hide
      MSP430_20.2.8.LTS*
      C6000_8.5.1.LTS*
      MSP430_21.6.2.LTS*
      C29_1.0.2.LTS*
      C2000_22.6.3.LTS*
      ARMCLANG_3.2.4.LTS*
      ARMCLANG_4.0.4.LTS
      PRU_2.3.4*
      C6000_8.3.15*
      C7000_5.0.2.LTS*
      C2000_21.6.2.LTS*
      ARMCLANG_5.0.0.LTS*
      Show
      MSP430_20.2.8.LTS* C6000_8.5.1.LTS* MSP430_21.6.2.LTS* C29_1.0.2.LTS* C2000_22.6.3.LTS* ARMCLANG_3.2.4.LTS* ARMCLANG_4.0.4.LTS PRU_2.3.4* C6000_8.3.15* C7000_5.0.2.LTS* C2000_21.6.2.LTS* ARMCLANG_5.0.0.LTS*
    • default

      At link-time, when attempting to consolidate DWARF debug frame information (i.e. the contents of the .debug_frame section), the linker can, in some cases, generate incorrect addresses for information contained in a Frame Description Entry (FDE) for a given function.

      For example, consider the debug frame information for a main() function in an object file that is input to the linker:

      Function: main
      Length: 28
      CIE Pointer: 00000000
      Initial Location: 0x00000000
      Address Range: 88
      State Table:
      0x00000000 CFA:R13
      0x00000002 CFA:R13+20
      R4->[R13]
      R5->[R13+4]
      R6->[R13+8]
      R7->[R13+12]
      R14->[R13+16]
      0x00000004 CFA:R13+48
      R4->[R13+28]
      R5->[R13+32]
      R6->[R13+36]
      R7->[R13+40]
      R14->[R13+44]

      Note: Such information about a function can be displayed using the following command on an ELF object file:

      > tiarmofd -g --obj_display=none --dwarf_display=none,dframe main.o > main_fde.txt

      Now consider the FDE for the main() function from the linked output file:

      Function: main
      Length: 36
      CIE Pointer: 00000000
      Initial Location: 0x000019a4
      Address Range: 88
      State Table:
      0x000019a4 CFA:R13
      0x000019a4 CFA:R13+20
      R4->[R13]
      R5->[R13+4]
      R6->[R13+8]
      R7->[R13+12]
      R14->[R13+16]
      0x000019a4 CFA:R13+48
      R4->[R13+28]
      R5->[R13+32]
      R6->[R13+36]
      R7->[R13+40]
      R14->[R13+44]
      0x000019f0 CFA:R13+48
      R4->[R13+28]
      R5->[R13+32]
      R6->[R13+36]
      R7->[R13+40]
      R14->[R13+44]

      Note that the first three Call Frame Address (CFA) entries are annotated with the same address. This is incorrect and does not correspond with the information that was obtained from the object file that contains the definition of main(). The linker should have advanced the CFA addresses for main() in the linked output in the same manner as was done for the input object file.

      The above information can be obtained from the linked output file using a similar tiarmofd command as mentioned earlier:

      > tiarmofd -g --obj_display=none --dwarf_display=none,dframe a.out > a_frames.txt

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5950 - Dwarf call frame information contai...
                ERROR
                • Last Sync Date: