Project debug doesn't work for Am62A

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-2667
    • CCS_20.3.0
    • CCS_21.0.0
    • None

      Project name: uart_echo_am62ax-sk_mcu-r5fss0-0_nortos_ti-arm-clang

      Project debug doesn't work, I get a message saying 'no compatible core found'.

      Seems like some sort of mismatch between core names.

      From the ccxml file:
      ```
       <subpath id="A53SS0_CORE0">
                                  <cpu HW_revision="1.0" XML_version="1.2" desc="A53SS0_CORE0_0" description="A53SS0 A53 Core 0" id="CortexA53_0" isa="CortexA53"/>
      ```
      Looks like Debug Server is returning A53SS0_CORE0, while Project Server is returning A53SS0_CORE0_0. Not sure which one is correct, need to investigate.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5919 - Project debug doesn't work for Am62A
                SYNCHRONIZED
                • Last Sync Date: