When debug view is closed, it cannot be reopened via View menu

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-2668
    • CCS_20.3.0
    • CCS_21.1.0
    • None

      When the debug view is closed from the left panel, It cannot be reopened from the View menu (View > Debug > [any item here]). Clicking one of the debug view menu items will activate the view if it's already opened, but does nothing if the view is closed. Workaround is opening view from command palette.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5918 - When debug view is closed, it canno...
                SYNCHRONIZED
                • Last Sync Date: