Wrong base address in Can_RegisterReadback API

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      Bug Description:
      In Can_RegisterReadback interface to read register values, the base address used by the interface is directly offset from the Ram area base address rather than the Register address.

      Register addresses as follows

      But Register Read back base address is as follows

      Rootcause:
      Base address generated from configurator is directly used. But the base addresses are different for subsystem registers and core registers which shall be calculated based on the can controller base address.
      Workaround:
      Use functions MCAN_SsAddr and MCAN_CfgAddr to fetch sub system and config register addresses respectively

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5906 - Wrong base address in Can_RegisterR...
                SYNCHRONIZED
                • Last Sync Date: