CSI-2 Rx driver shall support frame width that is not 16-byte-aligned

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Linux Core SDK
    • LCPD-43976
    • 11.00
    • 11.02
    • Hide
      am62axx_sk-fs
      am62pxx_sk-fs
      am62xx_sk-fs
      Show
      am62axx_sk-fs am62pxx_sk-fs am62xx_sk-fs

      The CSI-2 Rx driver (j721e-csi2rx) has a limitation of frame width being a multiple of 16 bytes:

      https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/drivers/media/platform/ti/j721e-csi2rx/j721e-csi2rx.c?h=ti-linux-6.12.y#n370

      However, there is no such limitation in HW IP. Some applications such as lidar have frame widths that are not a multiple of 16 bytes. Therefore, this limitation shall be removed from CSI-2 Rx driver.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5815 - CSI-2 Rx driver shall support frame...
                ERROR
                • Last Sync Date: