Unable to debug project when project folder is added to the workspace

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Composer Studio Theia
    • CCSNXT-2603
    • CCS_20.2.0
    • CCS_20.3.0
    • None

      Unable to debug project when project folder is explicitly added to the workspace via "Add Folder to Workspace..."

      The issue appears to be due to the .theia folder (containing the launch.json file) being generated in the parentt folder of the project folder instead of inside the project folder.

      Moving the .theia folder into the project folder will allow the launch to succeed.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5785 - Unable to debug project when projec...
                SYNCHRONIZED
                • Last Sync Date: