Endless loop of "Force Reset" dialog prompts

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Debug and Trace
    • DBGTRC-7355
    • CCS_20.2.0
    • CCS_20.5.0
    • Generic

      Attempting to launch a debug session for an MSPM0L1307 LaunchPad using the XDS110ISO-EVM debug connection. Something is wrong with the connection and a dialog appears asking if a Force Reset should be performed. It has 2 buttons, OK and Force Reset. If the reset does not work the dialog is shown again. Clicking ok, X, or Force Reset just results in the dialog. being presented again. Even terminating the debug session does not exit this loop. Only way to clear it is to close CCS.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            1 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5628 - Endless loop of "Force Reset" dialo...
                SYNCHRONIZED
                • Last Sync Date: