Using --symbol_map with LTO results in incorrect optimizations across functions

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-9576
    • Hide
      ARMCLANG_5.0.0.STS
      ARMCLANG_4.0.0.LTS
      Show
      ARMCLANG_5.0.0.STS ARMCLANG_4.0.0.LTS
    • Hide
      ARMCLANG_5.0.0.STS
      ARMCLANG_4.0.5.LTS*
      Show
      ARMCLANG_5.0.0.STS ARMCLANG_4.0.5.LTS*
    • default

      When the linker --symbol_map option is used with Link-Time Optimization (LTO), the executable that results may execute incorrectly. This is because critical LTO optimizations may not applied correctly across remapped function definitions. This may result in important variables or functions being removed from the final link.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5625 - Using --symbol_map with LTO results...
                ERROR
                • Last Sync Date: