Extend multicam support to any channel mask instead of contiguous

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      Currently multi-cam application only supports consecutive channel mask and channel mask is calculated based on the num of cam enabled (i.e. 2 cam means ch_mask - 0x3)  

      When 2 cam connected at any ports are provided (i.e. ch_mask - 0x11), two changes has to be done additionally to the application.

      1. manually change ch_mask to 0x11 after the API app_querry_sensor()
      2. Modify the starting channel parameter in app_init_aewb() to take the respective ports as starting channel.

      This should be automatically done by the application based on the port the cam is connected in.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5547 - Extend multicam support to any chan...
                SYNCHRONIZED
                • Last Sync Date: