CC2340R5 using Car Node example was not identified by the BLE Agent package

XMLWordPrintable

    • Type: Bug
    • Resolution: Won't Fix
    • Priority: Medium
    • SimpleLink Lowpower SDK F3 BLE5 Stack
    • BLE_LOKI-3199
    • BLE_LOKI_9_10_00_RC16
    • BLE_LOKI_9_11_00
    • CC23XX
    • car node removed from R5

      Description: Car Node flashed on CC2340R5 is not identified by BLE Agent package. The error printed is "nodes not identified at all" and is originated by the exception BleDeviceNodesNotIdentifiedException, in method BleDevice.set_device. BLE Agent package now recognizes the CC2340R5 using Car Node example.

       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5493 - CC2340R5 using Car Node example was...
                SYNCHRONIZED
                • Last Sync Date: