GATT_Indication/GATT_Notification does not check link status if authentication is set to false

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SimpleLink Lowpower SDK F3 BLE5 Stack
    • BLE_LOKI-2493
    • BLE Stack BLE5-3.x.x
    • Hide
      BLE_LOKI_9_10_00
      BLE_LOKI_9_10_00_RC4
      Show
      BLE_LOKI_9_10_00 BLE_LOKI_9_10_00_RC4
    • CC23XX

      Description: In the GATT_Indication/GATT_Notification APIs, if the param authenticated is set to false, the host will not run the link status check.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5476 - GATT_Indication/GATT_Notification d...
                SYNCHRONIZED
                • Last Sync Date: