SDK DOC: Both MII ports still have to be enabled in single port case

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Linux Core SDK
    • LCPD-42593
    • Hide
      10.00
      10.01
      Show
      10.00 10.01
    • 11.00
    • Hide
      am64xx-evm
      am654x-idk
      Show
      am64xx-evm am654x-idk

      The Linux SDK docs claim that "Both MIIx ports have to be enabled in DT even if one of them is not used (no Ethernet PHY wired) for proper PRU_ICSSG Ethernet driver work. Use fixed-link for unused port as workaround." https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/10_01_10_04/exports/docs/linux/Foundational_Components/PRU-ICSS/Linux_Drivers/PRU_ICSSG_Ethernet.html

      That seems inaccurate and this shouldn't be the case.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5267 - SDK DOC: Both MII ports still have ...
                SYNCHRONIZED
                • Last Sync Date: