MacOS: missing symbol frmo Mac libc++.1.dylib may cause link to fail

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Generation Tools
    • CODEGEN-13642
    • Hide
      C29_1.0.0.LTS
      ARMCLANG_4.0.2.LTS
      Show
      C29_1.0.0.LTS ARMCLANG_4.0.2.LTS
    • Hide
      C29_2.0.0.STS*
      ARMCLANG_4.0.3.LTS
      Show
      C29_2.0.0.STS* ARMCLANG_4.0.3.LTS
    • default
    • Update the MacOS system version to 14.0 or later

      In MacOS versions 13 and prior, the affected toolchains may fail to link, citing a missing symbol from the libc++.1.dylib library. This is because the linker executable has been generated using a library from a more recent MacOS version.

      While this will be resolved in future releases and patches, the affected versions can only be used by updating the MacOS version to a more recent release.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5292 - MacOS: missing symbol frmo Mac libc...
                ERROR
                • Last Sync Date: