Fls Driver Does Not Support Multiple Sectors

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • MCAL
    • MCAL-27321
    • n/a
    • Hide
      MCAL_SitaraMPU_09.00.00.01
      MCUSW_J7_10.01.00
      Show
      MCAL_SitaraMPU_09.00.00.01 MCUSW_J7_10.01.00
    • Hide
      MCAL_SitaraMPU_11.01.00
      MCUSW_J7_11.01.00
      Show
      MCAL_SitaraMPU_11.01.00 MCUSW_J7_11.01.00
    • Hide
      am275x-evm
      am62a-evm
      am62d-evm
      am62p-evm
      am62x-evm
      j7200-evm
      j721e-evm
      j721s2-evm
      j722s-evm
      j742s2-evm
      j784s4-evm
      Show
      am275x-evm am62a-evm am62d-evm am62p-evm am62x-evm j7200-evm j721e-evm j721s2-evm j722s-evm j742s2-evm j784s4-evm

      The Fls driver does not support multiple sectors as required by the AUTOSAR Fee module. The issue is due to the hardcoded `SectorList` index as `1` in the driver code and the static definition of `SectorList` in `Fls.h`.

      This restricts the driver functionality and results in build failures if more than one sector is configured in EB Tresos. The limitation is hardcoded into the driver code, making it incompatible with the AUTOSAR Fee module, which requires multiple sectors to be configured.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5221 - Fls Driver Does Not Support Multipl...
                SYNCHRONIZED
                • Last Sync Date: