-
Type:
Enhancement
-
Resolution: Implemented
-
Priority:
Medium
-
Code Composer Studio Theia
-
CCSNXT-1494
-
CCS_20.0.0
-
CCS_20.2.0
-
None
Description: The installer prevent users to select a folder like "C:\Program Files (x86)\Texas Instruments" or "C:\Program Files\Texas Instruments" (or any other folder like "C:\Program Files\<folder>"). Installing in "C:\Program Files (x86)" or "C:\Program Files" works but leads all the installation files to be in the mentioned repository (which is not acceptable as it may lead to file naming conflicts and prevents the installation of more than one CCS version at the time)
Impact: The security policy in certain companies prevent program execution from outside "C:\Program Files (x86)" or "C:\Program Files". As a consequence, these users cannot install CCS.