Project wizard Example name input doesn't accept new name when using it for the second time

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Resource Explorer
    • REX-4025
    • Hide
      REX_4.21.0
      REX_4.20.0
      Show
      REX_4.21.0 REX_4.20.0
    • Generic

      An error shows up when changing the name for an example before clicking create in Project Wizard after creating a different example and changing its name successfully.

      It appears that the name input component is not updating properly, and not taking the new input inserted in the input field when the user tries to do that for the second time while using project wizard.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-5186 - Project wizard Example name input d...
                SYNCHRONIZED
                • Last Sync Date: