Capture terminates silently without user warning when user clicks on Home page

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Edge AI Studio
    • EDGEST-1267
    • MC_1.3.0
    • MC_1.4.0
    • None
    • Hide
      When you switch back observe that the Capture page is in the view files mode.
      Capture was interrupted and did not complete if it was in progress.
      The workaround is to avoid switching to the Home page during Capture or Live Preview.
      Show
      When you switch back observe that the Capture page is in the view files mode. Capture was interrupted and did not complete if it was in progress. The workaround is to avoid switching to the Home page during Capture or Live Preview.

      Start a Motor-fault or arc-fault capture that gives you enough time to switch to the Home page.
      When you open the same project observe that the Capture page is in the view files mode.
      Opening the capture mode shows that there is no capture happening.
      The capture and/or live preview session in progress was terminated by switching to the Home screen.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5133 - Capture terminates silently without...
                SYNCHRONIZED
                • Last Sync Date: