Graph: Need ability to explicitly specify the data type size

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: Medium

      It is not possible to explicitly set the data type size. CCS will default to the type of the varable/array specified. If an explicit address is used instead of an expression, it will default to the size of a word for the CPU. In cases where an explicit address is used, a custom type size should be able to be specified.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5087 - Graph: Need ability to explicitly s...
                SYNCHRONIZED
                • Last Sync Date: