AM654x: USB MSC boot mode fails

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Linux Core SDK
    • LCPD-24130
    • 08.00.00
    • 12.02.00
    • am654x-evm

      On AM654 USB MSC boot mode is failing. Errors are seen while reading from the USB storage drive. May be an issue with the phy tuning values

       

      U-Boot SPL 2021.01-00001-g3da5fdae37f0-dirty (Aug 25 2021 - 19:28:12 +0530)
      SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
      SPL initial stack usage: 7552 bytes
      Trying to boot from USB
             scanning usb for storage devices... 1 Storage Device(s) found
      WARN halted endpoint, queueing URB anyway.
      Unexpected XHCI event TRB, skipping... (41c72530 00000000 13000000 01008400)
      BUG at drivers/usb/host/xhci-ring.c:500/abort_td()!
      BUG!
      resetting ...
      
      

      May be an issue with USB2PHY tuning values

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-4993 - AM654x: USB MSC boot mode fails
                SYNCHRONIZED
                • Last Sync Date: