[Display]: Ethernet Firmware needs to be disabled for DP output

XMLWordPrintable

    • Type: Bug
    • Resolution: Cannot Reproduce
    • Priority: Medium
    • PDK
    • PDK-14695
    • Hide
      PROCESSOR_SDK_08.06.00
      PROCESSOR_SDK_09.00.00
      Show
      PROCESSOR_SDK_08.06.00 PROCESSOR_SDK_09.00.00
    • PROCESSOR_SDK_11.01.00
    • Hide
      j721e-evm
      j784s4-evm
      Show
      j721e-evm j784s4-evm
    • Hide
      Unable to reproduce with latest code.
      Verified with the 11.1 at SDK level and it is working
      Show
      Unable to reproduce with latest code. Verified with the 11.1 at SDK level and it is working

      Description
      The io expander pin, which controls power for the DP convertor, is enabled only when EthFw is disabled, even though this io expander uses i2c1, which is not used for EthFw.

      Workaround
      Disable EthFw for DP usecase

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4910 - [Display]: Ethernet Firmware needs ...
                SYNCHRONIZED
                • Last Sync Date: