J784S4: U-Boot: DFU boot broken with R5 default defconfig

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent
    • Linux Core SDK
    • LCPD-42151
    • 09.02.00
    • 10.00
    • j784s4-hsevm
    • SDK 10.0 . Keeping tiboot3 size to 512KB

      In SDK 9.2, the size of the R5 binary has increased and incase of USB DFU boot if binary size exceeds 512KB then it appears that the ROM is failing to load the tiboot3.bin. (No logs can be seen at all in console)

      WA:
      When tiboot3.bin size is reduced by removing some config options, ROM is able to load the execute the R5 SPL.

      Remove CONFIG_SPL_FS_LOADER option from r5 defconfig to get USB DFU working

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4833 - J784S4: U-Boot: DFU boot broken wit...
                SYNCHRONIZED
                • Last Sync Date: