Add tooltip with more information regarding sync groups

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-1924
    • CCS_THEIA_1.5.1
    • CCS_20.0.0
    • None

      Synchronous groups have very specific behavior and should be used for specific scenarios. Many people are not aware of this and hence there is high risk of misusing this functionality. In CCS Eclipse, there was a very specific popup that provides more details.

      There is no such information with CCS Theia. I feel this is needed for clarity. A tooltip when hovering over the checkbox for it should be adequate.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4834 - Add tooltip with more information r...
                SYNCHRONIZED
                • Last Sync Date: