[LINUX] Array test case failing with migration to latest Linux GCC compiler

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Low
    • OpenVX Framework
    • TIOVX-1782
    • TIOVX_10.00.00
    • TDA54.12.01.00.00
    • Hide
      j721e-evm
      j721s2-evm
      j784s4-evm
      j722s-evm
      j742s2-evm
      tda54-evm
      Show
      j721e-evm j721s2-evm j784s4-evm j722s-evm j742s2-evm tda54-evm

      The Array test case is failing with the migration to the new Linux compiler

      The case statement in the function doing the verification (own_verify_data_items) has an issue where the switch statement does not properly go to the correct condition

      Note: when changing from optimization "-o3" to "-o2", this issue is not seen

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4714 - [LINUX] Array test case failing wit...
                SYNCHRONIZED
                • Last Sync Date: