vxSetGraphParameterByIndex does not conform to pipelining spec

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • OpenVX Framework
    • TIOVX-1700
    • TIOVX_09.02.00
    • TIOVX_10.01.00

      From version 3.1 the functionality of vxSetGraphParameterByIndex was clarified; no change in functionality was intended, but the resulting specification meant that there is a bug with TIOVX.

      The specification now reads:

      7.7. Framework: Graph Parameters

      Defines the Graph Parameter API.

      Graph parameters allow Clients to create graphs with Client settable input/output parameters. A graph parameter

      inherits its attributes from the node parameter used to create it [REQ-1965]. The vx_parameter object is first retrieved

      from a node in the graph via vxGetParameterByIndex and then set as a graph parameter via vxAddParameterToGraph

      function.

      The vxSetGraphParameterByIndex function sets a reference object to graph parameter, which in turn set this

      parameter on originating node as well as any other connected nodes in the graph. The application must guarantee

      that none of the input graph parameters have a connection from another node’s output parameter. If the application

      violates this restriction, the behavior is implementation-defined.

       

      The bolded section is the problem.  TIOVX sets the reference object only on the single node originally given when the graph parameter was added.

      It’s not sufficient to change all occurrences of the same reference on nodes in the graph, because at the time of graph verification they need not have been the same reference; therefore a list of nodes connected to a graph parameter is constructed at the time the graph is verified and this is used to assign a new reference correctly when vxSetGraphParameterByIndex is called.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4754 - vxSetGraphParameterByIndex does not...
                SYNCHRONIZED
                • Last Sync Date: