Assembler error when ISR built with interrupt_save_fp dumped and compiled as assembly.

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      When using the "interrupt_save_fp" function attribute, which includes floating point status registers among the register context that is saved and restored, a debug line is generated that thwarts the assembler.

      epwm_register_write.s:329:9: error: invalid register in register list
      .save {fpscr, fpexc}
      

      This happens when -save-temps is used, where the compiler will dump a generated assembly file and then assemble that file.  

      -S can also be used to dump the generated assembly, though this is not compiled.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4617 - Assembler error when ISR built with...
                ERROR
                • Last Sync Date: