GEL errors when using CC2340R5 on Linux

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      When using UniFlash 8.7 Linux with CC2340R5, the below errors occur:

      [12/06/2024, 10:28:34] [ERROR] Cortex_M0P: Trouble Setting Breakpoint with the Action "Terminate GEL_Go()" at 0xf002505: (Error -1066 @ 0xF002504) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 12.7.0.00130)
      [12/06/2024, 10:28:34] [ERROR] Cortex_M0P: GEL: Error while executing OnTargetConnect(): An earlier error prevented the target from running at GEL_Go(entryPoint) [cc23xx_xds.gel:55] at OnTargetConnect()

      The same UniFlash version and device on Windows does not have these errors.

      The issue does not occur with older UniFlash version like 8.3. It is not known which exact version this issue was introduced.

      When using CCS 12.7.0 Linux with the same device, the program can be flashed without errors also.

      Issue reproduced with UniFlash Linux on Ubuntu 24.04 and 22.04.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4596 - GEL errors when using CC2340R5 on L...
                SYNCHRONIZED
                • Last Sync Date: