-
Type:
Bug
-
Resolution: Fixed
-
Priority:
High
-
SimpleLink Lowpower SDK F3 BLE5 Stack
-
BLE_LOKI-1653
-
BLE Stack BLE5-3.3.1 RC4
-
-
CC23XX
Description of the issue: When Initiator receives aux_scan_rsp with unknown address, instead of sending "last command done" and let the stack decide if it's a valid address, it ignore the packet and keep scanning. The peripheral act as the connection is established.
Steps to reproduce the issue:
- Set the initiator Resolvable Private Address Timeout to 5 seconds or less.
- Set Create connection command with privacy.
- The peripheral will advertise but with wrong IRK.
- The connection should not be established.
- Wait at least 5 seconds.
- The peripheral will now advertise with correct IRK
- The connection now should be established but will fail.