J722S QNX: Conformance test failures observed due to cache issue in QNX

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • OpenVX Framework
    • TIOVX-1511
    • TIOVX_09.01.01
    • TIOVX_11.00.00
    • j722s-evm

      J722S QNX: Conformance test failures observed due to cache issue in QNX.

      Note: this is seen across both C7X and R5F with core conformance and the hwa tests, respectively

      Latest notes on this from debug on 3/5:

      • Not consistently reproducible.  Have run the vxAddSub tests through and can get a failure after several tests, but not until all previous tests are all run
      • If I change the sizes of the buffers, it doesn't seem to occur more consistently.  As I increase the size of the buffers, it happens less
      • Played around with location of shared memory but that didn't seem to help/cause any deltas
      • It doesn't occur at a consistent physical address
      • Tried using wbinv but that didn't help

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4445 - J722S QNX: Conformance test failure...
                SYNCHRONIZED
                • Last Sync Date: