In Can_PBcfg.c file CAN_START_SEC_ISR_CODE defined prior to CAN_STOP_SEC_CONFIG_DATA

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • MCAL
    • MCAL-22599
    • -
    • MCUSW_J7_09.00.00
    • Hide
      MCUSW_J7_10.00.00
      MCAL_SitaraMPU_10.00.00
      Show
      MCUSW_J7_10.00.00 MCAL_SitaraMPU_10.00.00
    • Hide
      am62a-evm
      am62p-evm
      am62x-evm
      j7200-evm
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      am62a-evm am62p-evm am62x-evm j7200-evm j721e-evm j721s2-evm j784s4-evm

      Hello team,

      In post build configuration after generating CAN configuration,Can_PBcfg.c file has CAN_START_SEC_ISR_CODE defined prior to CAN_STOP_SEC_CONFIG_DATA.

      Whereas in pre-compile configuration Can_cfg.c file, CAN_START_SEC_ISR_CODE defined after CAN_STOP_SEC_CONFIG_DATA.

      As per AUTOSAR Specification, it has to be as in Pre-compile configuration please correct it.

      Post Build:

      Pre Compile:

      Regards
      Tarun Mukesh

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4433 - In Can_PBcfg.c file CAN_START_SEC_I...
                SYNCHRONIZED
                • Last Sync Date: