ETH: Corruption of ethernet frame due to checksum info not cleared in descriptor for non IPv4, IPv6 frames

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • MCAL
    • MCAL-21039
    • NA
    • MCUSW_J7_09.00.00
    • MCUSW_J7_09.02.00
    • Hide
      j7200-evm
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j7200-evm j721e-evm j721s2-evm j784s4-evm

      Checksum info in descriptor is not cleared, while submitting the packet to UDMA.
      Which might pass old checksum info to CPSW Host Port, if old checksum info have some data then it will corrupt the packet result corrupted packet will be sent out of External Port to outside network.

      Fix: We need to clear the checksum info for the packet, to which checksum calculation is not required.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4428 - ETH: Corruption of ethernet frame d...
                SYNCHRONIZED
                • Last Sync Date: