For WKUP_GPIO ,DIO channels from 32 to 42 are reserved

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • MCAL
    • MCAL-20060
    • NA
    • MCUSW_J7_09.00.00
    • MCUSW_J7_09.02.00
    • Hide
      j7200-evm
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j7200-evm j721e-evm j721s2-evm j784s4-evm

      Hello,

      In Dio configuration file for J784S4,

      we have a condition to reserve the pins from 32 to 42,
      [!IF "num:i(DioChannelId) >= num:i('32') and num:i(DioChannelId) <= num:i('42')"!][!ERROR "Configured Pin is Reserved"!][!ENDIF!]

      whereas in TRM or datasheet , we don't have those pins as reserved

      Please correct this and check all the platforms of jacinto and request to correct this

      Regards
      Tarun Mukesh

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4429 - For WKUP_GPIO ,DIO channels from 32...
                SYNCHRONIZED
                • Last Sync Date: