-
Type:
Bug
-
Resolution: Unresolved
-
Priority:
Medium
-
SimpleLink CC13x2-26x2 SDK BLE5 Stack
-
BLE_AGAMA-4837
-
BLE Stack BLE5-2.2.9 RC7
-
BLE Stack BLE5-2.2.11
-
Devices: CC26X2R, CC1354P10-1
OS: Android 14 on One Plus 11
Compiler: TICLANG and IAR
RTOS: TIRTOS
Last working version- OS: Android 13
Description:
Connecting and pairing (read characteristic 5) to simple peripheral with phone (only with One Plus 11) on Android 14. After bond completes, if phone disconnects and reconnects, then the reconnection will fail.
Note:
- The bond saved on the phone
- With Android 12- there is no bug. The phone successfully reconnects.
- With Android 14 and another phone (not One Plus, for example, Galaxy 23 or Google Pixel 7), there is no bug.
- If flashed hex with public address- behavior is not observed