BLE Stack does not dequeue ATT msg during fuzzing test

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-4425
    • BLE Stack BLE5-2.2.8 RC12
    • Hide
      BLE Stack BLE5-2.2.9
      BLE Stack BLE5-2.2.9 RC7
      BLE Stack BLE5-2.2.9 RC9
      Show
      BLE Stack BLE5-2.2.9 BLE Stack BLE5-2.2.9 RC7 BLE Stack BLE5-2.2.9 RC9
    • CC26X2R1

      When performing fuzzing test, it is observed that eventually the stack will get stuck in a loop where it is not able to successfully dequeue ATT msgs. During test, if the device enqueues a lot of ATT msgs and suddenly terminates a connection, the enqueued msgs are not dequeued.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4413 - BLE Stack does not dequeue ATT msg ...
                SYNCHRONIZED
                • Last Sync Date: