[CC2642] Peripheral fails to respond to CON_IND when using GAP_ADV_WL_POLICY_WL_ALL_REQ and connected to Central using RPA with Random ID

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-4573
    • Hide
      BLE Stack BLE5-2.2.7
      BLE Stack BLE5-2.2.4
      BLE Stack BLE5-2.2.5
      Show
      BLE Stack BLE5-2.2.7 BLE Stack BLE5-2.2.4 BLE Stack BLE5-2.2.5
    • Hide
      BLE Stack BLE5-2.2.9
      BLE Stack BLE5-2.2.9 RC1
      Show
      BLE Stack BLE5-2.2.9 BLE Stack BLE5-2.2.9 RC1

      When connecting a peripheral device that is using the GAP_ADV_WL_POLICY_WL_ALL_REQ filter option in SysConfig with a Central device that is using the RPA with Random ID addressing mode, the peripheral is observed to not respond to the received CONN_IND packet from central. This is observed in a reconnection and not the initial connection

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4411 - [CC2642] Peripheral fails to respon...
                SYNCHRONIZED
                • Last Sync Date: