-
Type:
Bug
-
Resolution: Fixed
-
Priority:
Urgent
-
SimpleLink CC13x2-26x2 SDK BLE5 Stack
-
BLE_AGAMA-4710
-
BLE Stack BLE5-2.2.9 RC1
-
-
CC1354P10_1
On the CC1354P10-1, the device fails to save the 16th bond when acting as a peripheral and the 15th bond when acting as a central. In other words, when the CC1354P10-1 is operating in peripheral (such as simple_peripheral), it will be able to successfully form 15 bonds, but fail when forming the 16th bond. When operating in central mode (using simple_central), then the behavior is seen on the 15th bond.