CLI Erase command for MSP430Gx will erase calibration data in INFOA memory

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium

      By default, CLI Erase command for MSP430Gx will erase calibration data in INFOA memory

      ex: dslite.bat -c MSP430G2452.ccxml -b Erase

      It will perform a Mass Erase that will erase all of main memory and information memory segments A-D. Calibration data is in stored in segment A.

      This is likely not desired behavior for the default.

      Note that the same exact command in UniFlash 4.6 (using the same ccxml file) does NOT erase segment A. This is likely the desired default behavior.

      There seems to be some regression. I'm not sure if it is a UniFlash issue or if it is an issue with the Mass Erase functionality.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-4394 - CLI Erase command for MSP430Gx will...
                SYNCHRONIZED
                • Last Sync Date: