internal error generated for function with both vector code and struct param passed by value

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-11940
    • Hide
      C7000_1.4.0.LTS
      C7000_2.1.0.LTS
      C7000_3.1.0.LTS
      C7000_4.1.0.LTS
      Show
      C7000_1.4.0.LTS C7000_2.1.0.LTS C7000_3.1.0.LTS C7000_4.1.0.LTS
    • Hide
      C7000_4.1.2.LTS*
      C7000_6.1.0.STS
      C7000_5.0.1.LTS
      Show
      C7000_4.1.2.LTS* C7000_6.1.0.STS C7000_5.0.1.LTS
    • default
    • Rewrite the function arguments to pass the struct by pointer, not by value.

      The compiler may generate an internal error if a function which takes a struct parameter has any vector operations in the body of the function. This internal error does not occur if the struct is passed by pointer rather than by value.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4374 - internal error generated for functi...
                SYNCHRONIZED
                • Last Sync Date: