[VHWA] Error is incorrectly returns in the Udma_PopRing API of all Vhwa drivers

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-13305
    • NA
    • PROCESSOR_SDK_09.00.00
    • PROCESSOR_SDK_09.01.00
    • Hide
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j721e-evm j721s2-evm j784s4-evm

      Fixed issue. PopRings implementation updated to repeatedly try to dequeue an element from the output ring till successful. If dequeue is unsuccessful after 'n' attempts the driver reports an error using GT_Trace error statements.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4327 - [VHWA] Error is incorrectly returns...
                SYNCHRONIZED
                • Last Sync Date: