Reserved pins mismatch in DIO configuration file for WKUP_GPIO0

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • MCAL
    • MCAL-15304
    • MCUSW_J7_03.00.00
    • MCUSW_J7_09.02.00
    • Hide
      j721s2-evm
      j784s4-evm
      Show
      j721s2-evm j784s4-evm

      Hi team,

      In J721S2 SDK8.6 MCAL Example Dio_Lcfg.c configuration file , .reservedPinStart for WKUP_GPIO0 is configured as '32' instead of '89' based on TRM(screenshot added below) .Due to this configuration mistake , customers are facing issues across multiple modules configuring the DIO Pins. Once such example is the default can_app example is reporting DET errors while running and when i debugged into the application , it is due to DIO reserved pin mistake .After correcting the .reservedPinStart to 89 the issue got resolved.

      Please correct this and also check for remaining GPIO as well.

      Regards
      Tarun Mukesh

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4276 - Reserved pins mismatch in DIO confi...
                SYNCHRONIZED
                • Last Sync Date: